ExternalConnectionElementBuilderStreamType Enumeration

NXOpen.Mechatronics.ExternalConnectionElementBuilder.StreamType is an alias for NXOpen.Mechatronics.ExternalConnectionElementBuilderStreamType

class NXOpen.Mechatronics.ExternalConnectionElementBuilderStreamType

Bases: object

the stream type.

Enum Members

Enum Member Enum Member Description
R
read
W
write
Rw
read and write
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.