ExternalConnectionElementBuilderDataType Enumeration

NXOpen.Mechatronics.ExternalConnectionElementBuilder.DataType is an alias for NXOpen.Mechatronics.ExternalConnectionElementBuilderDataType

class NXOpen.Mechatronics.ExternalConnectionElementBuilderDataType

Bases: object

the data type.

Enum Members

Enum Member Enum Member Description
Unknown
unknown
Integer
integer
Float
float
Boolean
boolean
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.