ExternalConnectionBuilderConditionType Enumeration¶
NXOpen.Mechatronics.ExternalConnectionBuilder.ConditionType is an alias for NXOpen.Mechatronics.ExternalConnectionBuilderConditionType
-
class
NXOpen.Mechatronics.
ExternalConnectionBuilderConditionType
¶ Bases:
object
the condition type.
Deprecated since version NX8.0.1: Please use
NXOpen.Mechatronics.ExternalConnectionElementBuilder
instead.Enum Members
Enum Member Enum Member Description Eq equalGt greater thanLt less thanGe greater than or equalLe less than or equalNe not equal-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-