ExpressionBlockFormulaCollection Class¶
-
class
NXOpen.Mechatronics.
ExpressionBlockFormulaCollection
¶ Bases:
object
Represents a collection of ExpressionBlock Formula.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateExpressionBlockFormulaBuilder | Creates a NXOpen.Mechatronics.ExpressionBlockFormulaBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ExpressionBlockFormula with the given name. |
Method Detail¶
CreateExpressionBlockFormulaBuilder¶
-
ExpressionBlockFormulaCollection.
CreateExpressionBlockFormulaBuilder
¶ Creates a
NXOpen.Mechatronics.ExpressionBlockFormulaBuilder
.Signature
CreateExpressionBlockFormulaBuilder(expressionBlockFormula)
Parameters: expressionBlockFormula ( NXOpen.Mechatronics.ExpressionBlockFormula
) –NXOpen.Mechatronics.ExpressionBlockFormula
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ExpressionBlockFormulaBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ExpressionBlockFormulaCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ExpressionBlockFormula
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ExpressionBlockFormula
.Returns: NXOpen.Mechatronics.ExpressionBlockFormula
with this name.Return type: NXOpen.Mechatronics.ExpressionBlockFormula
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)