ElectricalPartCollection Class

class NXOpen.Mechatronics.ElectricalPartCollection

Bases: object

Represents a NXOpen.Mechatronics.ElectricalPartCollection

To obtain an instance of this class, refer to NXOpen.Mechatronics.MechatronicsManager

New in version NX9.0.0.

Methods

Method Description
CreateElectricalPartBuilder Create builder for ElectricalPart class @return NXOpen.Mechatronics.ElectricalPart object
FindObject Finds the NXOpen.Mechatronics.ElectricalPart object with the given name.

Method Detail

CreateElectricalPartBuilder

ElectricalPartCollection.CreateElectricalPartBuilder

Create builder for ElectricalPart class

Signature CreateElectricalPartBuilder(object)

Parameters:object (NXOpen.Mechatronics.ElectricalPart) – NXOpen.Mechatronics.ElectricalPart to be edited, if None then create a new one
Returns:NXOpen.Mechatronics.ElectricalPart object
Return type:NXOpen.Mechatronics.ElectricalPartBuilder

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

ElectricalPartCollection.FindObject

Finds the NXOpen.Mechatronics.ElectricalPart object with the given name.

Signature FindObject(name)

Parameters:name (str) – Name of the object, actually it shall be handle.
Returns:NXOpen.Mechatronics.ElectricalPart object with this name.
Return type:NXOpen.Mechatronics.ElectricalPart

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)