ECADImportBuilderPositionMode Enumeration¶
NXOpen.Mechatronics.ECADImportBuilder.PositionMode is an alias for NXOpen.Mechatronics.ECADImportBuilderPositionMode
-
class
NXOpen.Mechatronics.
ECADImportBuilderPositionMode
¶ Bases:
object
Represents the position mode.
Deprecated since version NX9.0.0: This enum type has no replacement. It is no longer supported.
Enum Members
Enum Member Enum Member Description InferredOnly Inferred OnlyAbsoluteOrigin Absolute OriginSelectOrigin Select OriginByConstraints By ConstraintsMove Move-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-