ECADExportBuilder Class¶
-
class
NXOpen.Mechatronics.
ECADExportBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ECADExportBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateECADExportBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ExportFile | Returns or sets the export file name |
ExportFileFormat | Returns or sets the export file format. |
SelectLogicals | Returns the selected logical objects. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExportAttributesName | Gets the exported attributes name @return Exported attributes name |
GetObject | Returns the object currently being edited by this builder. |
SetExportAttributesName | Sets the exported attributes name |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ECADExportBuilderExportFileType Enumeration | Represents the export file type. |
Property Detail¶
ExportFile¶
-
ECADExportBuilder.
ExportFile
¶ Returns or sets the export file name
-------------------------------------
Getter Method
Signature
ExportFile()
Returns: The export file name Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExportFile(exportFile)
Parameters: exportFile (str) – The export file name New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExportFileFormat¶
-
ECADExportBuilder.
ExportFileFormat
¶ Returns or sets the export file format.
-------------------------------------
Getter Method
Signature
ExportFileFormat()
Returns: Return type: NXOpen.Mechatronics.ECADExportBuilderExportFileType
New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ExportFileFormat(exportFileFormat)
Parameters: exportFileFormat ( NXOpen.Mechatronics.ECADExportBuilderExportFileType
) –New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectLogicals¶
-
ECADExportBuilder.
SelectLogicals
¶ Returns the selected logical objects.
This can be a
NXOpen.Mechatronics.LogicObject
.-------------------------------------
Getter Method
Signature
SelectLogicals()
Returns: Array of selected logical objects Return type: NXOpen.Mechatronics.SelectLogicObjectList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
GetExportAttributesName¶
-
ECADExportBuilder.
GetExportAttributesName
¶ Gets the exported attributes name
Signature
GetExportAttributesName()
Returns: Exported attributes name Return type: list of str New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetExportAttributesName¶
-
ECADExportBuilder.
SetExportAttributesName
¶ Sets the exported attributes name
Signature
SetExportAttributesName(exportAttributesName)
Parameters: exportAttributesName (list of str) – Exported attributes name New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ECADExportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.