DistanceSensorBuilder Class¶
-
class
NXOpen.Mechatronics.
DistanceSensorBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.DistanceSensor
builder.To create a new instance of this class, use
NXOpen.Mechatronics.DistanceSensorCollection.CreateDistanceSensorBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Angle |
|
Category |
|
Direction |
|
HighlightOnCollision |
|
LowerOutputRange |
|
MeasureType |
|
Name |
|
Point |
|
Range |
|
RigidBody |
|
Tag | Returns the Tag for this object. |
UpperOutputRange |
|
UseScale |
|
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DistanceSensorBuilderOutputMeasureType Enumeration |
|
Property Detail¶
Angle¶
-
DistanceSensorBuilder.
Angle
¶ Returns the open angle. The angle between the cone surface and the Direction.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Category¶
-
DistanceSensorBuilder.
Category
¶ Returns or sets the category. It should be between 0 and 16.
-------------------------------------
Getter Method
Signature
Category()
Returns: Return type: int New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Category(category)
Parameters: category (int) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Direction¶
-
DistanceSensorBuilder.
Direction
¶ Returns or sets the direction. The Distance Sensor has the scope of a cone. The direction is the vector of the cone.
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
HighlightOnCollision¶
-
DistanceSensorBuilder.
HighlightOnCollision
¶ Returns or sets the option of highlight on collision. If the highlight is true, then the sensor will be highlighted when it is collided or triggered during simulation.
-------------------------------------
Getter Method
Signature
HighlightOnCollision()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
HighlightOnCollision(highlight)
Parameters: highlight (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerOutputRange¶
-
DistanceSensorBuilder.
LowerOutputRange
¶ Returns the lower output range used to scale the distance data. Its measure type contains constant, voltage, current
-------------------------------------
Getter Method
Signature
LowerOutputRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MeasureType¶
-
DistanceSensorBuilder.
MeasureType
¶ Returns or sets the measure type.
-------------------------------------
Getter Method
Signature
MeasureType()
Returns: Return type: NXOpen.Mechatronics.DistanceSensorBuilderOutputMeasureType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MeasureType(measureType)
Parameters: measureType ( NXOpen.Mechatronics.DistanceSensorBuilderOutputMeasureType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
DistanceSensorBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Point¶
-
DistanceSensorBuilder.
Point
¶ Returns or sets the point. Sensor Reference Point, also used as start point to measure the distance
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Range¶
-
DistanceSensorBuilder.
Range
¶ Returns the range of distance sensor. Also as the height of the cone
-------------------------------------
Getter Method
Signature
Range()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RigidBody¶
-
DistanceSensorBuilder.
RigidBody
¶ Returns the Rigid Body. This can be a
NXOpen.Mechatronics.RigidBody
If there is a rigid body, then the sensor will move with the rigid body.-------------------------------------
Getter Method
Signature
RigidBody()
Returns: Return type: NXOpen.Mechatronics.SelectRigidBody
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperOutputRange¶
-
DistanceSensorBuilder.
UpperOutputRange
¶ Returns the upper output range used to scale the distance data.
-------------------------------------
Getter Method
Signature
UpperOutputRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseScale¶
-
DistanceSensorBuilder.
UseScale
¶ Returns or sets the use scale flag, which is used to control if the distance sensor includes scale parameters.
-------------------------------------
Getter Method
Signature
UseScale()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseScale(useScale)
Parameters: useScale (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
DistanceSensorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.