ComparisonResultContext Class

class NXOpen.Mechatronics.ComparisonResultContext

Bases: NXOpen.Mechatronics.ComparisonResultBase

Represents context of comparison results

New in version NX9.0.0.

Properties

Property Description
EcadProjectId Returns the ECAD project ID from the comparison context
Ignored Returns or sets the flag marked if the object will be ingored when applying it to logical model
PartName Returns the part name from the comparison context

Methods

Method Description
Dispose Frees the object from memory.
GetResults Gets a list of comparison results from the context
ResolveConflictResult Generates some new results to resolve the conflict

Enumerations

ComparisonResultContextResolveConflictAction Enumeration Defines actions for resolving conflicts

Property Detail

EcadProjectId

ComparisonResultContext.EcadProjectId

Returns the ECAD project ID from the comparison context

-------------------------------------

Getter Method

Signature EcadProjectId()

Returns:Project ID of ECAD model
Return type:str

New in version NX9.0.0.

License requirements: None.

PartName

ComparisonResultContext.PartName

Returns the part name from the comparison context

-------------------------------------

Getter Method

Signature PartName()

Returns:Name of logical model part
Return type:str

New in version NX9.0.0.

License requirements: None.

Method Detail

Dispose

ComparisonResultContext.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX9.0.0.

License requirements: None.

GetResults

ComparisonResultContext.GetResults

Gets a list of comparison results from the context

Signature GetResults()

Returns:Array of results
Return type:list of NXOpen.Mechatronics.ComparisonResult

New in version NX9.0.0.

License requirements: None.

ResolveConflictResult

ComparisonResultContext.ResolveConflictResult

Generates some new results to resolve the conflict

Signature ResolveConflictResult(conflictResult, action)

Parameters:
Returns:

Array of new generated results

Return type:

list of NXOpen.Mechatronics.ComparisonResult

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)