ComparisonResultAttribute Class

class NXOpen.Mechatronics.ComparisonResultAttribute

Bases: NXOpen.Mechatronics.ComparisonResultBase

Represents attribute of comparison result

New in version NX9.0.0.

Properties

Property Description
EcadValue Returns or sets the value of imported ECAD device object
Ignored Returns or sets the flag marked if the object will be ingored when applying it to logical model
LogicalValue Returns or sets the value of matched logical object
Name Returns the name of the attribute

Methods

Method Description
Dispose Frees the object from memory.

Property Detail

EcadValue

ComparisonResultAttribute.EcadValue

Returns or sets the value of imported ECAD device object

-------------------------------------

Getter Method

Signature EcadValue()

Returns:Value of imported ECAD device object
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EcadValue(ecadValue)

Parameters:ecadValue (str) – Value of imported ECAD device object

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

LogicalValue

ComparisonResultAttribute.LogicalValue

Returns or sets the value of matched logical object

-------------------------------------

Getter Method

Signature LogicalValue()

Returns:Value of matched logical object
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LogicalValue(logicalValue)

Parameters:logicalValue (str) – Value of matched logical object

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

Name

ComparisonResultAttribute.Name

Returns the name of the attribute

-------------------------------------

Getter Method

Signature Name()

Returns:Name of attribute
Return type:str

New in version NX9.0.0.

License requirements: None.

Method Detail

Dispose

ComparisonResultAttribute.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX9.0.0.

License requirements: None.