CamProfileBuilderProfileCyclicType Enumeration¶
NXOpen.Mechatronics.CamProfileBuilder.ProfileCyclicType is an alias for NXOpen.Mechatronics.CamProfileBuilderProfileCyclicType
-
class
NXOpen.Mechatronics.
CamProfileBuilderProfileCyclicType
¶ Bases:
object
Indicates which cyclic type should be take.
The type of Cam Profile can be switched between non-cyclic, cyclic and relative cyclic
Enum Members
end point of the profile do not necessarily have to be equal. “
“Cyclic”, ” In Cyclic Cam Profiles the points at the beginningand the end of the Master Axis range need to be identical with respect to Slave Axis value, slope and curve.”
“NonCyclic”, ” Non-cyclic Cam Profiles are defined only inthe defined master axis range. Exceeding this range will cause an error.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-