BreakingConstraintBuilderBreakingModeType Enumeration

NXOpen.Mechatronics.BreakingConstraintBuilder.BreakingModeType is an alias for NXOpen.Mechatronics.BreakingConstraintBuilderBreakingModeType

class NXOpen.Mechatronics.BreakingConstraintBuilderBreakingModeType

Bases: object

Represents the breaking mode.

Enum Members

Enum Member Enum Member Description
Force
Force
Torque
Torque
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.