AngularLimitJointCollection Class¶
-
class
NXOpen.Mechatronics.
AngularLimitJointCollection
¶ Bases:
object
Represents a collection of Angular Limit Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateAngularLimitJointBuilder | Creates a NXOpen.Mechatronics.AngularLimitJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.AngularLimitJoint with the given name. |
Method Detail¶
CreateAngularLimitJointBuilder¶
-
AngularLimitJointCollection.
CreateAngularLimitJointBuilder
¶ Creates a
NXOpen.Mechatronics.AngularLimitJointBuilder
.Signature
CreateAngularLimitJointBuilder(angularLimit)
Parameters: angularLimit ( NXOpen.Mechatronics.AngularLimitJoint
) –NXOpen.Mechatronics.AngularLimitJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.AngularLimitJointBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
AngularLimitJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.AngularLimitJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.AngularLimitJoint
.Returns: NXOpen.Mechatronics.AngularLimitJoint
with this name.Return type: NXOpen.Mechatronics.AngularLimitJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)