AccelerometerCollection Class¶
-
class
NXOpen.Mechatronics.
AccelerometerCollection
¶ Bases:
object
Represents a collection of Accelerometer.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateAccelerometerBuilder |
|
FindObject |
|
Method Detail¶
CreateAccelerometerBuilder¶
-
AccelerometerCollection.
CreateAccelerometerBuilder
¶ Creates a
NXOpen.Mechatronics.AccelerometerBuilder
.Signature
CreateAccelerometerBuilder(accelerometer)
Parameters: accelerometer ( NXOpen.Mechatronics.Accelerometer
) –NXOpen.Mechatronics.Accelerometer
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.AccelerometerBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
AccelerometerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.Accelerometer
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.Accelerometer
.Returns: NXOpen.Mechatronics.Accelerometer
with this name.Return type: NXOpen.Mechatronics.Accelerometer
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)