State Enumeration¶
-
class
NXOpen.Layer.
State
¶ Bases:
object
Represents the state of the layer Enum Members
Enum Member Enum Member Description WorkLayer Work layer. All newly created objects are placed on the work layer.Selectable Objects on the layer are selectableVisible Objects on the layer are visible but not selectableHidden Objects on the layer are not visible and not selectable-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-