Constants Enumeration¶
-
class
NXOpen.Layer.
Constants
¶ Bases:
object
Constants for layers Enum Members
Valid layers are numbered from
LayerConstants.FirstLayer
toLayerConstants.LastLayer
““LastLayer”, ” The number of the last layer.Valid layers are numbered from
LayerConstants.FirstLayer
toLayerConstants.LastLayer
“-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-