ImageCaptureBuilderImageSize Enumeration¶
NXOpen.Gateway.ImageCaptureBuilder.ImageSize is an alias for NXOpen.Gateway.ImageCaptureBuilderImageSize
-
class
NXOpen.Gateway.
ImageCaptureBuilderImageSize
¶ Bases:
object
the image size
Enum Members
Enum Member Enum Member Description Pixels16 the 16 pixel sizePixels24 the 24 pixel sizePixels32 the 32 pixel sizePixels48 the 48 pixel sizePixels64 the 64 pixel sizePixels96 the 96 pixel sizePixels128 the 128 pixel size-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-