ImageCaptureBuilderImageFormat Enumeration¶
NXOpen.Gateway.ImageCaptureBuilder.ImageFormat is an alias for NXOpen.Gateway.ImageCaptureBuilderImageFormat
-
class
NXOpen.Gateway.
ImageCaptureBuilderImageFormat
¶ Bases:
object
the image format
Enum Members
Enum Member Enum Member Description Bmp the bmp image formatJpg the jpg image formatGif the gif image formatPng the png image formatTiff the tiff image format-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-