CopyCutBuilderStatus Enumeration¶
NXOpen.Gateway.CopyCutBuilder.Status is an alias for NXOpen.Gateway.CopyCutBuilderStatus
-
class
NXOpen.Gateway.
CopyCutBuilderStatus
¶ Bases:
object
Status of Copy or Cut Operation
Enum Members
Enum Member Enum Member Description NoObjectsCopied No objects were successfully copiedNonExportableObjects Certain non-exportable objects were not copiedPartExportFailed Error while exporting part with copied/cut objectsErrorDuringCut Error during the cut operationAllObjectsCopied All objects were successfully copied-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-