UpdateDiscrepancyType Enumeration¶
NXOpen.Formboard.UpdateDiscrepancy.Type is an alias for NXOpen.Formboard.UpdateDiscrepancyType
-
class
NXOpen.Formboard.
UpdateDiscrepancyType
¶ Bases:
object
The general type of the discrepancy.
Enum Members
- missing from the formboard. “
- “Extra”, ” Object is in the formboard but not in
- the 3D harness. “
- “Modified”, ” Object exists in both 3D and the formboard but
is modified in some way. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.