UpdateDiscrepancyObjectType Enumeration¶
NXOpen.Formboard.UpdateDiscrepancy.ObjectType is an alias for NXOpen.Formboard.UpdateDiscrepancyObjectType
-
class
NXOpen.Formboard.
UpdateDiscrepancyObjectType
¶ Bases:
object
Specifies the type of objects involved in the discrepancy.
Enum Members
- electrical connector. “
- “Component”, ” A component assigned as a
- electrical connector or device. “
- “Harness”, ” Harness. ” “Wire”, ” Wire connection. ” “Cable”, ” Cable connection. ” “Shield”, ” Shield connection. ” “Connector”, ” ConnectorDevice object which
- has a type of connector. “
- “Device”, ” ConnectorDevice object which
- has a type of device. “
- “Overstock”, ” Overstock. ” “Fillerstock”, ” Filler stock. ” “FittingOverstock”, ” Overstock applied to fittings. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.