OrientBranchBuilderBranchAngleMethod Enumeration¶
NXOpen.Formboard.OrientBranchBuilder.BranchAngleMethod is an alias for NXOpen.Formboard.OrientBranchBuilderBranchAngleMethod
-
class
NXOpen.Formboard.
OrientBranchBuilderBranchAngleMethod
¶ Bases:
object
Enum to define the type of method to orient branch.
Enum Members
Enum Member Enum Member Description AnglefromReferenceVector method to rotate branch with respect to selected vectors Angle method to rotate branch by angleAlignAxisToVector method to rotate branch by an angle between two vectorsTwoPoints method to rotate branch by and angle between two points-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-