LayoutLengthOptionsRoundingMethod Enumeration¶
NXOpen.Formboard.LayoutLengthOptions.RoundingMethod is an alias for NXOpen.Formboard.LayoutLengthOptionsRoundingMethod
-
class
NXOpen.Formboard.
LayoutLengthOptionsRoundingMethod
¶ Bases:
object
Methods of rounding lengths for Formboard geometry.
The rounding method determines the value of the length in the Formboard by modifying the original length values from the 3D harness part file.
Enum Members
- to the nearest increment value. “
- “UpToNearest”, ” Lengths are rounded up to the
- nearest increment value. “
- “DownToNearest”, ” Lengths are rounded down to
the nearest increment value. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.