FormboardLayoutBuilderMainRunType Enumeration¶
NXOpen.Formboard.FormboardLayoutBuilder.MainRunType is an alias for NXOpen.Formboard.FormboardLayoutBuilderMainRunType
-
class
NXOpen.Formboard.
FormboardLayoutBuilderMainRunType
¶ Bases:
object
Selection method for the set of segments that define the main run of the formboard geometry.
Enum Members
- thickest bundle. “
- “UserSelection”, ” Manual selection of path. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.