FormboardLayoutBuilderBranchAngle Enumeration¶
NXOpen.Formboard.FormboardLayoutBuilder.BranchAngle is an alias for NXOpen.Formboard.FormboardLayoutBuilderBranchAngle
-
class
NXOpen.Formboard.
FormboardLayoutBuilderBranchAngle
¶ Bases:
object
Methods for determining which angles to apply at each branch of the Formboard.
Enum Members
- of the branch in the 3D harness. “
- “StandardAngles”, ” Apply a standard angle to the branch,
the level of the branch determines which angle to apply. “
“MaximumAngles”, ” Apply the largest possible angle valuesat every branch to force the harness to spread out. “
“RandomAngles”, ” Randomly choose an angle for eachbranch. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.