FaceAnnotationBuilderTypes Enumeration¶
NXOpen.Formboard.FaceAnnotationBuilder.Types is an alias for NXOpen.Formboard.FaceAnnotationBuilderTypes
-
class
NXOpen.Formboard.
FaceAnnotationBuilderTypes
¶ Bases:
object
Enum which defines the type to import CGM/Pattern file
Enum Members
Enum Member Enum Member Description ComponentAttribute Import CGM file by selecting a componentCgmFileSelection Import CGM file by browsing a CGM filePatternFileSelection Import a pattern file-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-