FieldVariableBounds_Struct Struct¶
NXOpen.Fields.FieldVariable.Bounds is an alias for NXOpen.Fields.FieldVariableBounds_Struct
-
class
NXOpen.Fields.
FieldVariableBounds_Struct
¶ Bases:
object
Variable Bounds structure .
Constructor: NXOpen.Fields.FieldVariable.Bounds()
Fields¶
Field | Description |
---|---|
IsMinimumDefined | true if minimum bound is defined |
IsMinimumInclusive | true if minimum bound is inclusive |
MinimumValue | minimum bound value |
IsMaximumDefined | true if maximum bound is defined |
IsMaximumInclusive | true if maximum bound is inclusive |
MaximumValue | maximum bound value |
IsMinimumDefined¶
-
FieldVariableBounds_Struct.
IsMinimumDefined
¶ true if minimum bound is defined
-------------------------------------
Field Value Type:bool
IsMinimumInclusive¶
-
FieldVariableBounds_Struct.
IsMinimumInclusive
¶ true if minimum bound is inclusive
-------------------------------------
Field Value Type:bool
MinimumValue¶
-
FieldVariableBounds_Struct.
MinimumValue
¶ minimum bound value
-------------------------------------
Field Value Type:float
IsMaximumDefined¶
-
FieldVariableBounds_Struct.
IsMaximumDefined
¶ true if maximum bound is defined
-------------------------------------
Field Value Type:bool