FieldTableLoadFileOption Enumeration¶
NXOpen.Fields.FieldTable.LoadFileOption is an alias for NXOpen.Fields.FieldTableLoadFileOption
-
class
NXOpen.Fields.
FieldTableLoadFileOption
¶ Bases:
object
Load file options
Enum Members
Enum Member Enum Member Description Append Append data to the table removing duplicatesReplace Replace data removing duplicates-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-