FieldManager Class¶
-
class
NXOpen.Fields.
FieldManager
¶ Bases:
NXOpen.NXObject
Represents the manager class of the Fields
This manager class gives access to all the fields
NXOpen.Fields.Field
within a part, as well as the collection of domainsNXOpen.Fields.FieldDomain
.It also provides creation methods for the various builders of fields and related classes.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Domains |
|
Fields |
|
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
CreateComplexScalarFieldWrapperWithExpressions | Create a complex scalar field wrapper backed by two scalar expressions @return scalar field wrapper created and associated to the expression |
CreateComplexScalarFieldWrapperWithField | Create a complex scalar field wrapper backed up by a complex scalar field @return vector field wrapper created and associated to the field |
CreateDependentVariable | Create a dependent variable to be added to the field @return dependent variable created and associated to the field |
CreateDisplayPropertiesBuilder | Creates a NXOpen.Fields.DisplayPropertiesBuilder @return |
CreateExportData | Creates a Fields. |
CreateFieldExpression | Creates a system NXOpen.Fields.FieldExpression object. |
CreateFieldFormula | Creates a NXOpen.Fields.FieldFormula object with dependent NXOpen.Fields.FieldExpression . |
CreateFieldLink | Creates a NXOpen.Fields.FieldLink . |
CreateFieldLinksTable | Creates a NXOpen.Fields.FieldLinksTable object with dependent and independent variables NXOpen.Fields.FieldVariable . |
CreateFieldTable | Creates a NXOpen.Fields.FieldTable object with dependent and independent variables NXOpen.Fields.FieldVariable . |
CreateFieldTableFromData | Creates a NXOpen.Fields.FieldTable object with dependent and independent variables NXOpen.Fields.FieldVariable . |
CreateFieldWrapper | Create a field wrapper backed up by a field @return scalar field wrapper created and associated to the field |
CreateImportData | Creates a Fields. |
CreateIndependentVariable | Create an independent variable to be added to the field @return independent variable created and associated to the field |
CreateMeshSizeFieldData | Create Mesh Size Field NXOpen.Fields.Field object @return Created Field |
CreatePathObjects | Creates a NXOpen.Fields.PathObjects @return |
CreateScalarFieldWrapperWithExpression | Create a field wrapper backed by a scalar expression @return scalar field wrapper created and associated to the expression |
CreateScalarFieldWrapperWithField | Create a scalar field wrapper backed up by a scaled scalar field @return scalar field wrapper created and associated to the field |
CreateSpatialMapBuilder | Creates a NXOpen.Fields.SpatialMapBuilder @return |
CreateSubFieldExpression | Creates a system NXOpen.Fields.FieldExpression object with independent variables. |
CreateVectorFieldWrapperWithExpressions | Create a vector field wrapper backed by three scalar expressions @return scalar field wrapper created and associated to the expression |
CreateVectorFieldWrapperWithField | Create a vector field wrapper backed up by a scaled vector field @return vector field wrapper created and associated to the field |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteField | Deletes the specified NXOpen.Fields.Field object; if the object cannot be deleted it is returned. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EditDependentVariable | Edit dependent variable |
EditIndependentVariable | Edit an independent variable |
ExportFields | Exports fields to a text file as defined by export_data parameter |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNameVariable | Locate an existing, or create a new NXOpen.Fields.NameVariable object @return name variable with the specified measure and name |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetValidFieldId | Get the next available ID for NXOpen.Fields.Field object @return valid id |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
ImportFields | Imports fields from a text file as defined by import_data parameter |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
FieldManager.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FieldManager.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FieldManager.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FieldManager.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FieldManager.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FieldManager.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Domains¶
-
FieldManager.
Domains
¶ Returns a collection of Domains
Signature
Domains()
New in version NX3.0.0.
Returns: Return type: NXOpen.Fields.FieldDomainCollection
Fields¶
-
FieldManager.
Fields
¶ Returns a collection of Fields
Signature
Fields()
New in version NX11.0.0.
Returns: Return type: NXOpen.Fields.FieldCollection
Method Detail¶
CreateComplexScalarFieldWrapperWithExpressions¶
-
FieldManager.
CreateComplexScalarFieldWrapperWithExpressions
¶ Create a complex scalar field wrapper backed by two scalar expressions
Signature
CreateComplexScalarFieldWrapperWithExpressions(expressions)
Parameters: expressions (list of NXOpen.Expression
) – existing expressions that will be this wrapper’s valueReturns: scalar field wrapper created and associated to the expression Return type: NXOpen.Fields.ComplexScalarFieldWrapper
New in version NX11.0.0.
License requirements: None.
CreateComplexScalarFieldWrapperWithField¶
-
FieldManager.
CreateComplexScalarFieldWrapperWithField
¶ Create a complex scalar field wrapper backed up by a complex scalar field
Signature
CreateComplexScalarFieldWrapperWithField(field)
Parameters: field ( NXOpen.Fields.Field
) – an existing field that will be this wrapper’s valueReturns: vector field wrapper created and associated to the field Return type: NXOpen.Fields.ComplexScalarFieldWrapper
New in version NX11.0.0.
License requirements: None.
CreateDependentVariable¶
-
FieldManager.
CreateDependentVariable
¶ Overloaded method CreateDependentVariable
CreateDependentVariable(ownerField, nameVariable, unitType)
CreateDependentVariable(ownerField, nameVariable, unitType, type)
-------------------------------------
Create a dependent variable to be added to the field
Signature
CreateDependentVariable(ownerField, nameVariable, unitType)
Parameters: - ownerField (
NXOpen.Fields.Field
) – owner field - nameVariable (
NXOpen.Fields.NameVariable
) – existing name variable - unitType (
NXOpen.Unit
) – unit of the dependent variable
Returns: dependent variable created and associated to the field
Return type: New in version NX6.0.2.
License requirements: None.
-------------------------------------
Create a dependent variable to be added to the field, specifying the variable value type
Signature
CreateDependentVariable(ownerField, nameVariable, unitType, type)
Parameters: - ownerField (
NXOpen.Fields.Field
) – owner field - nameVariable (
NXOpen.Fields.NameVariable
) – existing name variable - unitType (
NXOpen.Unit
) – unit of the dependent variable - type (
NXOpen.Fields.FieldVariableValueType
) – variable value type
Returns: dependent variable created and associated to the field
Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
CreateDisplayPropertiesBuilder¶
-
FieldManager.
CreateDisplayPropertiesBuilder
¶ Creates a
NXOpen.Fields.DisplayPropertiesBuilder
Signature
CreateDisplayPropertiesBuilder(fieldArray)
Parameters: fieldArray (list of NXOpen.Fields.Field
) – fields to edit display propertiesReturns: Return type: NXOpen.Fields.DisplayPropertiesBuilder
New in version NX6.0.1.
License requirements: None.
CreateExportData¶
-
FieldManager.
CreateExportData
¶ Creates a Fields.
ExportData
Signature
CreateExportData()
Returns: the export data created Return type: NXOpen.Fields.ExportData
New in version NX6.0.0.
License requirements: None.
CreateFieldExpression¶
-
FieldManager.
CreateFieldExpression
¶ Overloaded method CreateFieldExpression
CreateFieldExpression(fieldExpString, unitType)
CreateFieldExpression(fieldExpString, unitType, indepVarArray)
-------------------------------------
Creates a system
NXOpen.Fields.FieldExpression
object. Specifies the new expression string.Signature
CreateFieldExpression(fieldExpString, unitType)
Parameters: - fieldExpString (str) – expression string to be associated with the field
- unitType (
NXOpen.Unit
) – unit of the field
Returns: field
Return type: New in version NX4.0.0.
License requirements: None.
-------------------------------------
Creates a system
NXOpen.Fields.FieldExpression
object with independent variables. Specifies the new expression string.This method is deprecated; field expressions are children of
NXOpen.Fields.FieldFormula
and should not be created independently.Signature
CreateFieldExpression(fieldExpString, unitType, indepVarArray)
Parameters: - fieldExpString (str) – expression string to be associated with the field
- unitType (
NXOpen.Unit
) – unit of the field - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field
Returns: field
Return type: New in version NX4.0.0.
Deprecated since version NX10.0.0: Field expressions are owned by other objects. They are managed by the creation and editing of the owning object and should not be created independently.
License requirements: None.
-------------------------------------
CreateFieldFormula¶
-
FieldManager.
CreateFieldFormula
¶ Creates a
NXOpen.Fields.FieldFormula
object with dependentNXOpen.Fields.FieldExpression
.Signature
CreateFieldFormula(fieldName, indepVarArray, depExpArray)
Parameters: - fieldName (str) – field name
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depExpArray (list of
NXOpen.Fields.FieldExpression
) – dependent expression fields to be associated with the formula field
Returns: field
Return type: New in version NX6.0.0.
License requirements: None.
CreateFieldLink¶
-
FieldManager.
CreateFieldLink
¶ Creates a
NXOpen.Fields.FieldLink
.Signature
CreateFieldLink(fieldName, fieldToLink)
Parameters: - fieldName (str) – field name
- fieldToLink (
NXOpen.Fields.Field
) – field to link
Returns: field
Return type: New in version NX6.0.0.
License requirements: None.
CreateFieldLinksTable¶
-
FieldManager.
CreateFieldLinksTable
¶ Creates a
NXOpen.Fields.FieldLinksTable
object with dependent and independent variablesNXOpen.Fields.FieldVariable
.Signature
CreateFieldLinksTable(fieldName, indepVarArray, depVarArray, datapoints, linkFieldsArray)
Parameters: - fieldName (str) – field name
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables of this and all linked fields - datapoints (list of float) – row based array of double values representing the first independent variable; the number of points should equal the number of rows.
- linkFieldsArray (list of
NXOpen.Fields.Field
) – row based array of link field values representing the table; the number of fields should equal the number of rows.
Returns: links table field
Return type: New in version NX9.0.0.
License requirements: None.
CreateFieldTable¶
-
FieldManager.
CreateFieldTable
¶ Creates a
NXOpen.Fields.FieldTable
object with dependent and independent variablesNXOpen.Fields.FieldVariable
.Signature
CreateFieldTable(fieldName, indepVarArray, depVarArray, datapoints)
Parameters: - fieldName (str) – field name
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the table field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables to be associated with the table field - datapoints (list of float) – row based array of double values representing the table; then number of points should equal the number of independent variables * the number of dependent variables * the number of rows.
Returns: field
Return type: New in version NX6.0.0.
License requirements: None.
CreateFieldTableFromData¶
-
FieldManager.
CreateFieldTableFromData
¶ Creates a
NXOpen.Fields.FieldTable
object with dependent and independent variablesNXOpen.Fields.FieldVariable
.This will create a 2 dimensional table, with the option to specify the value type for the dependent variable.
Signature
CreateFieldTableFromData(fieldNamePrefix, ivarUnit, dvarUnit, dvarType, datapoints)
Parameters: - fieldNamePrefix (str) – field name prefix; e.g. “AFU Record”; field will have a unique generated name begining with this string
- ivarUnit (
NXOpen.Unit
) – unit of the independent variable - dvarUnit (
NXOpen.Unit
) – unit of the dependent variable - dvarType (
NXOpen.Fields.FieldVariableValueType
) – dependent variable type (real/imaginary/complex...) - datapoints (list of float) – row based array of double values representing the table; then number of points should equal the number of independent variables * the number of dependent variables * the number of rows.
Returns: field
Return type: New in version NX7.5.2.
License requirements: None.
CreateFieldWrapper¶
-
FieldManager.
CreateFieldWrapper
¶ Create a field wrapper backed up by a field
Signature
CreateFieldWrapper(field)
Parameters: field ( NXOpen.Fields.Field
) – an existing field that will be this wrapper’s valueReturns: scalar field wrapper created and associated to the field Return type: NXOpen.Fields.FieldWrapper
New in version NX6.0.0.
License requirements: None.
CreateImportData¶
-
FieldManager.
CreateImportData
¶ Creates a Fields.
ImportData
Signature
CreateImportData()
Returns: the import data created Return type: NXOpen.Fields.ImportData
New in version NX6.0.0.
License requirements: None.
CreateIndependentVariable¶
-
FieldManager.
CreateIndependentVariable
¶ Overloaded method CreateIndependentVariable
CreateIndependentVariable(ownerField, nameVariable, unitType, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
CreateIndependentVariable(ownerField, nameVariable, unitType, type, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
-------------------------------------
Create an independent variable to be added to the field
Signature
CreateIndependentVariable(ownerField, nameVariable, unitType, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
Parameters: - ownerField (
NXOpen.Fields.Field
) – owner field - nameVariable (
NXOpen.Fields.NameVariable
) – existing name variable - unitType (
NXOpen.Unit
) – unit of the independent variable - minValueSet (bool) – logical value whether minimum value set
- minValueInclusive (bool) – minimum value is itself included in range
- minValue (float) – minimum value of the variable range
- maxValueSet (bool) – logical value whether maximum value set
- maxValueInclusive (bool) – maximum value is itself included in range
- maxValue (float) – maximum value of the variable range
- numPtsSet (bool) – logical value whether num_pts set
- numPts (int) – num_pts of the variable range
- defaultValueSet (bool) – logical value whether default value set
- defaultValue (float) – default value of the variable range
Returns: independent variable created and associated to the field
Return type: New in version NX6.0.2.
License requirements: None.
-------------------------------------
Create an independent variable to be added to the field, specifying the variable value type
Signature
CreateIndependentVariable(ownerField, nameVariable, unitType, type, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
Parameters: - ownerField (
NXOpen.Fields.Field
) – owner field - nameVariable (
NXOpen.Fields.NameVariable
) – existing name variable - unitType (
NXOpen.Unit
) – unit of the independent variable - type (
NXOpen.Fields.FieldVariableValueType
) – variable value type - minValueSet (bool) – logical value whether minimum value set
- minValueInclusive (bool) – minimum value is itself included in range
- minValue (float) – minimum value of the variable range
- maxValueSet (bool) – logical value whether maximum value set
- maxValueInclusive (bool) – maximum value is itself included in range
- maxValue (float) – maximum value of the variable range
- numPtsSet (bool) – logical value whether num_pts set
- numPts (int) – num_pts of the variable range
- defaultValueSet (bool) – logical value whether default value set
- defaultValue (float) – default value of the variable range
Returns: independent variable created and associated to the field
Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
CreateMeshSizeFieldData¶
-
FieldManager.
CreateMeshSizeFieldData
¶ Create Mesh Size Field
NXOpen.Fields.Field
objectSignature
CreateMeshSizeFieldData(elementSizeType, meshArray)
Parameters: - elementSizeType (int) – At Centroid of Element Free Face and Elements=0, At Centroid of Element Free Faces=1, At Centroid of Elements=2
- meshArray (list of
NXOpen.TaggedObject
) –
Returns: Created Field
Return type: New in version NX11.0.0.
License requirements: None.
CreatePathObjects¶
-
FieldManager.
CreatePathObjects
¶ Creates a
NXOpen.Fields.PathObjects
Signature
CreatePathObjects()
Returns: Return type: NXOpen.Fields.PathObjects
New in version NX6.0.1.
License requirements: None.
CreateScalarFieldWrapperWithExpression¶
-
FieldManager.
CreateScalarFieldWrapperWithExpression
¶ Create a field wrapper backed by a scalar expression
Signature
CreateScalarFieldWrapperWithExpression(expression)
Parameters: expression ( NXOpen.Expression
) – an existing expression that will be this wrapper’s valueReturns: scalar field wrapper created and associated to the expression Return type: NXOpen.Fields.ScalarFieldWrapper
New in version NX6.0.0.
License requirements: None.
CreateScalarFieldWrapperWithField¶
-
FieldManager.
CreateScalarFieldWrapperWithField
¶ Create a scalar field wrapper backed up by a scaled scalar field
Signature
CreateScalarFieldWrapperWithField(field, scaleFactor)
Parameters: - field (
NXOpen.Fields.Field
) – an existing field that will be this wrapper’s value - scaleFactor (float) – the field will be multiplied by this scale factor when being evaluated
Returns: scalar field wrapper created and associated to the field
Return type: New in version NX6.0.0.
License requirements: None.
- field (
CreateSpatialMapBuilder¶
-
FieldManager.
CreateSpatialMapBuilder
¶ Creates a
NXOpen.Fields.SpatialMapBuilder
Signature
CreateSpatialMapBuilder(spatialmap)
Parameters: spatialmap ( NXOpen.Fields.SpatialMap
) – Existing SpatialMap to edit; NULL to createReturns: Return type: NXOpen.Fields.SpatialMapBuilder
New in version NX6.0.0.
License requirements: None.
CreateSubFieldExpression¶
-
FieldManager.
CreateSubFieldExpression
¶ Creates a system
NXOpen.Fields.FieldExpression
object with independent variables.Specifies the new expression string.
This method is used to create sub expression fields for a
NXOpen.Fields.FieldFormula
.Signature
CreateSubFieldExpression(depVar)
Parameters: depVar ( NXOpen.Fields.FieldVariable
) – dependent variables to be associated with the fieldReturns: field Return type: NXOpen.Fields.FieldExpression
New in version NX6.0.0.
License requirements: None.
CreateVectorFieldWrapperWithExpressions¶
-
FieldManager.
CreateVectorFieldWrapperWithExpressions
¶ Create a vector field wrapper backed by three scalar expressions
Signature
CreateVectorFieldWrapperWithExpressions(expressions)
Parameters: expressions (list of NXOpen.Expression
) – existing expressions that will be this wrapper’s valueReturns: scalar field wrapper created and associated to the expression Return type: NXOpen.Fields.VectorFieldWrapper
New in version NX6.0.0.
License requirements: None.
CreateVectorFieldWrapperWithField¶
-
FieldManager.
CreateVectorFieldWrapperWithField
¶ Create a vector field wrapper backed up by a scaled vector field
Signature
CreateVectorFieldWrapperWithField(field, scaleFactors)
Parameters: - field (
NXOpen.Fields.Field
) – an existing field that will be this wrapper’s value - scaleFactors (list of float) – the field will be multiplied by this scale factor when being evaluated
Returns: vector field wrapper created and associated to the field
Return type: New in version NX6.0.0.
License requirements: None.
- field (
DeleteField¶
-
FieldManager.
DeleteField
¶ Deletes the specified
NXOpen.Fields.Field
object; if the object cannot be deleted it is returned.Signature
DeleteField(field)
Parameters: field ( NXOpen.Fields.Field
) – field to deleteReturns: If the field cannot be deleted, it is returned; if the field is deleted, this will be NULL Return type: NXOpen.Fields.Field
New in version NX6.0.0.
License requirements: None.
EditDependentVariable¶
-
FieldManager.
EditDependentVariable
¶ Overloaded method EditDependentVariable
EditDependentVariable(depVar, varName, unitType)
EditDependentVariable(depVar, unitType)
-------------------------------------
Edit dependent variable
Signature
EditDependentVariable(depVar, varName, unitType)
Parameters: - depVar (
NXOpen.Fields.FieldVariable
) – dep variable to edit - varName (str) – new name for variable, or NULL to skip updating name
- unitType (
NXOpen.Unit
) – new unit of the dependent variable
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Edit dependent variable
Signature
EditDependentVariable(depVar, unitType)
Parameters: - depVar (
NXOpen.Fields.FieldVariable
) – dep variable to edit - unitType (
NXOpen.Unit
) – new unit of the dependent variable
New in version NX11.0.0.
License requirements: None.
-------------------------------------
EditIndependentVariable¶
-
FieldManager.
EditIndependentVariable
¶ Overloaded method EditIndependentVariable
EditIndependentVariable(indepVar, varName, unitType, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
EditIndependentVariable(indepVar, unitType)
-------------------------------------
Edit an independent variable
Signature
EditIndependentVariable(indepVar, varName, unitType, minValueSet, minValueInclusive, minValue, maxValueSet, maxValueInclusive, maxValue, numPtsSet, numPts, defaultValueSet, defaultValue)
Parameters: - indepVar (
NXOpen.Fields.FieldVariable
) – indep var to edit - varName (str) – name of the independent variable to be created
- unitType (
NXOpen.Unit
) – unit of the independent variable - minValueSet (bool) – logical value whether minimum value set
- minValueInclusive (bool) – minimum value is itself included in range
- minValue (float) – minimum value of the variable range
- maxValueSet (bool) – logical value whether maximum value set
- maxValueInclusive (bool) – maximum value is itself included in range
- maxValue (float) – maximum value of the variable range
- numPtsSet (bool) – logical value whether num_pts set
- numPts (int) – num_pts of the variable range
- defaultValueSet (bool) – logical value whether default value set
- defaultValue (float) – default value of the variable range
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Edit an independent variable
Signature
EditIndependentVariable(indepVar, unitType)
Parameters: - indepVar (
NXOpen.Fields.FieldVariable
) – indep var to edit - unitType (
NXOpen.Unit
) – unit of the independent variable
New in version NX11.0.0.
License requirements: None.
-------------------------------------
ExportFields¶
-
FieldManager.
ExportFields
¶ Exports fields to a text file as defined by export_data parameter
Signature
ExportFields(exportData)
Parameters: exportData ( NXOpen.Fields.ExportData
) – Export dataNew in version NX6.0.0.
License requirements: None.
FindObject¶
-
FieldManager.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetNameVariable¶
-
FieldManager.
GetNameVariable
¶ Locate an existing, or create a new
NXOpen.Fields.NameVariable
objectSignature
GetNameVariable(variableName, measureName)
Parameters: - variableName (str) – alphanumeric string; if it matches an existing name variable, the measures must also match
- measureName (str) – must match an existing measure name, or “Unitless”
Returns: name variable with the specified measure and name
Return type: New in version NX6.0.2.
License requirements: None.
GetValidFieldId¶
-
FieldManager.
GetValidFieldId
¶ Get the next available ID for
NXOpen.Fields.Field
objectSignature
GetValidFieldId()
Returns: valid id Return type: int New in version NX9.0.0.
License requirements: None.
ImportFields¶
-
FieldManager.
ImportFields
¶ Imports fields from a text file as defined by import_data parameter
Signature
ImportFields(importData)
Parameters: importData ( NXOpen.Fields.ImportData
) – Import dataNew in version NX6.0.0.
License requirements: None.
Print¶
-
FieldManager.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FieldManager.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.