FieldEvaluatorValuesOutsideTableInterpolationEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.ValuesOutsideTableInterpolationEnum is an alias for NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
-
class
NXOpen.Fields.
FieldEvaluatorValuesOutsideTableInterpolationEnum
¶ Bases:
object
Options for outside table values interpolation
Enum Members
Enum Member Enum Member Description Undefined No interpolation resultExtrapolate Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values usesConstant Returns the boundary value as interpolation result-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-