FieldEvaluatorInterpolationEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.InterpolationEnum is an alias for NXOpen.Fields.FieldEvaluatorInterpolationEnum
-
class
NXOpen.Fields.
FieldEvaluatorInterpolationEnum
¶ Bases:
object
Interpolation type
Enum Members
Enum Member Enum Member Description NotSet No interpolation method; table can only be used as a lookupLinear1d Standard linear interpolation between bounding pointsNearestNeighbor1d Locates the nearest point and returns its valueInverseDistanceWeighting1d Sum of the weighted value of all points, based on the inverse of the distanceDelaunay2dFast Triangulates the independent values and uses the bounding triangle, sacrifices accuracy for speedDelaunay2dMedium Triangulates the independent values and uses the bounding triangle, compromise between accuracy and speedDelaunay2dAccurate Triangulates the independent values and uses the bounding triangle, sacrifices speed for accuracyNearestNeighbor2d Locates the nearest point in a plane and returns its valueRenkaShepard2d Refined inverse distance weighting in 2D spaceInverseDistanceWeighting2d Sum of the weighted value of all points in 2D space, based on the inverse of the distanceDelaunay3dFast Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, sacrifices accuracy for speedDelaunay3dMedium Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, compromise between accuracy and speedDelaunay3dAccurate Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, sacrifices speed for accuracyNearestNeighbor3d Locates the nearest point in space and returns its valueRenkaShepard3d Refined inverse distance weighting in 3D spaceInverseDistanceWeighting3d Sum of the weighted value of all points in 3D space, based on the inverse of the distanceNearestNeighborNd Locates the nearest point in N dimensional space and returns its valueRenkaShepardNd Refined inverse distance weighting in N dimensional spaceInverseDistanceWeightingNd Sum of the weighted value of all points in N dimensional, based on the inverse of the distanceApproxNearestNeighbor2d Locates the approximate nearest point in a plane and returns its valueApproxNearestNeighbor3d Locates the approximate nearest point in space and returns its valueApproxNearestNeighborNd Locates the approximate nearest point in N dimensional space and returns its value-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-