WrapBuilderTypes Enumeration¶
NXOpen.Features.WrapBuilder.Types is an alias for NXOpen.Features.WrapBuilderTypes
-
class
NXOpen.Features.
WrapBuilderTypes
¶ Bases:
object
Settings for the type of wrap operation being performed.
Enum Members
- during edit you can get this value but any change will be ignored. “
- “Unwrap”, ” Curves are to be unwrapped from the selected faces onto the tangent plane,
during edit you can get this value but any change will be ignored. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.