WaveLinkBuilder Class¶
-
class
NXOpen.Features.
WaveLinkBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Wavelink Feature builder.
Inputs to this class can be convergent objects.
To create a new instance of this class, use
NXOpen.Features.BaseFeatureCollection.CreateWaveLinkBuilder()
Default values.
Property Value Associative True CompositeCurveBuilder.AllowSelfIntersection False CompositeCurveBuilder.Associative True CompositeCurveBuilder.CurveFitData.CurveJoinMethod No CompositeCurveBuilder.CurveFitData.Degree 7 CompositeCurveBuilder.CurveFitData.FitMethod DegreeAndSegments CompositeCurveBuilder.CurveFitData.IsAdvancedFit 0 CompositeCurveBuilder.CurveFitData.IsAlignShape 0 CompositeCurveBuilder.CurveFitData.MaximumDegree 7 CompositeCurveBuilder.CurveFitData.MaximumSegments 1 CompositeCurveBuilder.CurveFitData.MinimumDegree 5 CompositeCurveBuilder.CurveFitData.Segments 1 CompositeCurveBuilder.HideOriginal False CompositeCurveBuilder.InheritDisplayProperties False CopyThreads True ExtractFaceBuilder.AngleTolerance 45.0 ExtractFaceBuilder.Associative True ExtractFaceBuilder.CopyThreads True ExtractFaceBuilder.DeleteHoles False ExtractFaceBuilder.FixAtCurrentTimestamp False ExtractFaceBuilder.InheritDisplayProperties False ExtractFaceBuilder.IsPsmOutputBody false ExtractFaceBuilder.MakePositionIndependent False ExtractFaceBuilder.ReplacementAssistant.OneToOne True MirrorBodyBuilder.Associative True MirrorBodyBuilder.CopyThreads True MirrorBodyBuilder.FixAtCurrentTimestamp True MirrorBodyBuilder.InheritDisplayProperties False MirrorBodyBuilder.MakePositionIndependent False MirrorBodyBuilder.ParentPartType WorkPart MirrorBodyBuilder.ReplacementAssistant.OneToOne True WaveDatumBuilder.Associative True WaveDatumBuilder.DisplayScale 2.0 WaveDatumBuilder.InheritDisplayProperties False WaveDatumBuilder.ParentPart OtherPart WavePointBuilder.Associative True WavePointBuilder.DrawLineBetweenPoints False WavePointBuilder.InheritDisplayProperties False WavePointBuilder.ParentPart OtherPart WaveRoutingBuilder.Associative True WaveSketchBuilder.Associative True WaveSketchBuilder.InheritDisplayProperties False New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
BlankOriginal | Returns or sets the blank original |
CompositeCurveBuilder | Returns the composite curve builder |
CopyThreads | Returns or sets the copy threads option |
ExtractFaceBuilder | Returns or sets the extractfacebuilder |
FixAtCurrentTimestamp | Returns or sets the fix at timestamp option |
MakePositionIndependent | Returns or sets the make position independent option |
MirrorBodyBuilder | Returns or sets the mirrorbodybuilder |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
WaveDatumBuilder | Returns or sets the wave datum builder |
WavePointBuilder | Returns or sets the wave point builder |
WaveRoutingBuilder | Returns or sets the wave routing builder |
WaveSketchBuilder | Returns or sets the wave sketch builder |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WaveLinkBuilderTypes Enumeration | Wave Linker type |
Property Detail¶
Associative¶
-
WaveLinkBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BlankOriginal¶
-
WaveLinkBuilder.
BlankOriginal
¶ Returns or sets the blank original
-------------------------------------
Getter Method
Signature
BlankOriginal()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankOriginal(blankoriginal)
Parameters: blankoriginal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CompositeCurveBuilder¶
-
WaveLinkBuilder.
CompositeCurveBuilder
¶ Returns the composite curve builder
-------------------------------------
Getter Method
Signature
CompositeCurveBuilder()
Returns: Return type: NXOpen.Features.CompositeCurveBuilder
New in version NX5.0.0.
License requirements: None.
CopyThreads¶
-
WaveLinkBuilder.
CopyThreads
¶ Returns or sets the copy threads option
-------------------------------------
Getter Method
Signature
CopyThreads()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyThreads(copyThreads)
Parameters: copyThreads (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ExtractFaceBuilder¶
-
WaveLinkBuilder.
ExtractFaceBuilder
¶ Returns or sets the extractfacebuilder
-------------------------------------
Getter Method
Signature
ExtractFaceBuilder()
Returns: Return type: NXOpen.Features.ExtractFaceBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtractFaceBuilder(extractFaceBuilder)
Parameters: extractFaceBuilder ( NXOpen.Features.ExtractFaceBuilder
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FixAtCurrentTimestamp¶
-
WaveLinkBuilder.
FixAtCurrentTimestamp
¶ Returns or sets the fix at timestamp option
-------------------------------------
Getter Method
Signature
FixAtCurrentTimestamp()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixAtCurrentTimestamp(timestamp)
Parameters: timestamp (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MakePositionIndependent¶
-
WaveLinkBuilder.
MakePositionIndependent
¶ Returns or sets the make position independent option
-------------------------------------
Getter Method
Signature
MakePositionIndependent()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakePositionIndependent(makePositionIndependent)
Parameters: makePositionIndependent (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MirrorBodyBuilder¶
-
WaveLinkBuilder.
MirrorBodyBuilder
¶ Returns or sets the mirrorbodybuilder
-------------------------------------
Getter Method
Signature
MirrorBodyBuilder()
Returns: Return type: NXOpen.Features.MirrorBodyBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorBodyBuilder(mirrorBodyBuilder)
Parameters: mirrorBodyBuilder ( NXOpen.Features.MirrorBodyBuilder
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
WaveLinkBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.WaveLinkBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.WaveLinkBuilderTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
WaveDatumBuilder¶
-
WaveLinkBuilder.
WaveDatumBuilder
¶ Returns or sets the wave datum builder
-------------------------------------
Getter Method
Signature
WaveDatumBuilder()
Returns: Return type: NXOpen.Features.WaveDatumBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaveDatumBuilder(wavedatumBuilder)
Parameters: wavedatumBuilder ( NXOpen.Features.WaveDatumBuilder
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
WavePointBuilder¶
-
WaveLinkBuilder.
WavePointBuilder
¶ Returns or sets the wave point builder
-------------------------------------
Getter Method
Signature
WavePointBuilder()
Returns: Return type: NXOpen.Features.WavePointBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WavePointBuilder(wavepointBuilder)
Parameters: wavepointBuilder ( NXOpen.Features.WavePointBuilder
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
WaveRoutingBuilder¶
-
WaveLinkBuilder.
WaveRoutingBuilder
¶ Returns or sets the wave routing builder
-------------------------------------
Getter Method
Signature
WaveRoutingBuilder()
Returns: Return type: NXOpen.Features.WaveRoutingBuilder
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaveRoutingBuilder(waveroutingBuilder)
Parameters: waveroutingBuilder ( NXOpen.Features.WaveRoutingBuilder
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
WaveSketchBuilder¶
-
WaveLinkBuilder.
WaveSketchBuilder
¶ Returns or sets the wave sketch builder
-------------------------------------
Getter Method
Signature
WaveSketchBuilder()
Returns: Return type: NXOpen.Features.WaveSketchBuilder
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaveSketchBuilder(wavesketchBuilder)
Parameters: wavesketchBuilder ( NXOpen.Features.WaveSketchBuilder
) –New in version NX5.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
WaveLinkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.