WaveDatumBuilderParentPartType Enumeration

NXOpen.Features.WaveDatumBuilder.ParentPartType is an alias for NXOpen.Features.WaveDatumBuilderParentPartType

class NXOpen.Features.WaveDatumBuilderParentPartType

Bases: object

enum for scope of part

Enum Members

Enum Member Enum Member Description
WorkPart
intra part mode
OtherPart
inter part mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.