VirtualCurveBuilderTypes Enumeration¶
NXOpen.Features.VirtualCurveBuilder.Types is an alias for NXOpen.Features.VirtualCurveBuilderTypes
-
class
NXOpen.Features.
VirtualCurveBuilderTypes
¶ Bases:
object
the type of virtual curve
Enum Members
Enum Member Enum Member Description RotationAxis Rotation axisBlendCenterline Blend centerlineVirtualIntersection Virtual intersection-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-