WheelCoveringBuilderSurfaceSectionType Enumeration¶
NXOpen.Features.VehicleDesign.WheelCoveringBuilder.SurfaceSectionType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType
-
class
NXOpen.Features.VehicleDesign.
WheelCoveringBuilderSurfaceSectionType
¶ Bases:
object
Represents the type of the surface section.
Enum Members
Enum Member Enum Member Description CircleSection The checking surface is created as circle section typeAdr42 The checking surface is created as ADR 42 typeExtrudeSection The checking surface is created as extrude section type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-