WheelCoveringBuilderRequirementsControlType Enumeration

NXOpen.Features.VehicleDesign.WheelCoveringBuilder.RequirementsControlType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderRequirementsControlType

class NXOpen.Features.VehicleDesign.WheelCoveringBuilderRequirementsControlType

Bases: object

Represents the requirements control types to define the wheel covering.

Enum Members

Enum Member Enum Member Description
StandardDriven
Represents the option for reading parameters from the config file
UserDefined
Represents the option for input of user defined parameters
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.