WheelCoveringBuilderPositionType Enumeration

NXOpen.Features.VehicleDesign.WheelCoveringBuilder.PositionType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderPositionType

class NXOpen.Features.VehicleDesign.WheelCoveringBuilderPositionType

Bases: object

Represents the wheel covering positions.

Enum Members

Enum Member Enum Member Description
Front
Creates checking surface for front wheel only
Rear
Creates checking surface for rear wheel only
Both
Creates checking surface for both front and rear wheels
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.