TireEnvelopeBuilderTireDefinitionOption Enumeration

NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.TireDefinitionOption is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderTireDefinitionOption

class NXOpen.Features.VehicleDesign.TireEnvelopeBuilderTireDefinitionOption

Bases: object

Settings to indicate how the tire profile will be defined.

Enum Members

Enum Member Enum Member Description
SolidBody
Use a solid body.
ProfileCurves
Use curves in the current work part.
SketchfromOtherPart
Use curves from a sketch in another part.
ProfilePointFile
Read a text file with tire profile points.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.