TireEnvelopeBuilderSuspensionTemplateType Enumeration

NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.SuspensionTemplateType is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderSuspensionTemplateType

class NXOpen.Features.VehicleDesign.TireEnvelopeBuilderSuspensionTemplateType

Bases: object

Settings to indicate the defined suspension template to use.

Enum Members

Enum Member Enum Member Description
MacPhersonStrut
Use the MacPherson Strut suspension template.
ShortLongArmwithSteering
Use the Short-Long Arm with steering suspension template.
ShortLongArmwithoutSteering
Use the Short-Long Arm without steering suspension template.
FiveLinkSolidAxlewithoutSteering
Use the Five Link Solid Axle without steering suspension template.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.