TireEnvelopeBuilderSpindleFileLocationOption Enumeration

NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.SpindleFileLocationOption is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderSpindleFileLocationOption

class NXOpen.Features.VehicleDesign.TireEnvelopeBuilderSpindleFileLocationOption

Bases: object

Settings to indicate the location to select the spindle file.

Enum Members

Enum Member Enum Member Description
InNative
In Native
InTeamcenter
In Teamcenter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.