TireEnvelopeBuilderMotionMethod Enumeration¶
NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.MotionMethod is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderMotionMethod
-
class
NXOpen.Features.VehicleDesign.
TireEnvelopeBuilderMotionMethod
¶ Bases:
object
Settings to indicate how the suspension system motion will be defined.
Enum Members
Enum Member Enum Member Description ExistingSpindleFile From an existing spindle file.FromSpindleLines From lines that define the locations of the suspension components.ExistingScenarioMotionModel From an existing scenario motion model.SuspensionTemplate From a defined suspension template.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-