TireEnvelopeBuilderEnvelopeOffsetMethod Enumeration¶
NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.EnvelopeOffsetMethod is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderEnvelopeOffsetMethod
-
class
NXOpen.Features.VehicleDesign.
TireEnvelopeBuilderEnvelopeOffsetMethod
¶ Bases:
object
Settings to indicate how the offset will be defined.
Enum Members
Enum Member Enum Member Description FixedSections Use the values in the fixed sections.CustomerDefinedData Use the data that the user defines.FromOffsetFile From the offset file.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-