TireEnvelopeBuilderDriverGraphOption Enumeration

NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.DriverGraphOption is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderDriverGraphOption

class NXOpen.Features.VehicleDesign.TireEnvelopeBuilderDriverGraphOption

Bases: object

Settings to indicate the driver definition to use with the MacPherson Strut suspension template.

Enum Members

Enum Member Enum Member Description
RectangularJounceRebound
Use the rectangular jounce rebound definition.
RectangularTaperedY
Use the rectangular definition with taper in the Y direction.
RectangularTaperedX
Use the rectangular definition with taper in the X direction.
TaperedOneSide
Use the rectangular definition with taper on one side.
BySketch
Use a sketch to define the driver.
TwoDriversOneFixed
Use a fixed definition for two drivers.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.