SeatBeltAnchorageBuilderSeatPositionTypes Enumeration

NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilder.SeatPositionTypes is an alias for NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatPositionTypes

class NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatPositionTypes

Bases: object

the seat position type

Enum Members

Enum Member Enum Member Description
Left
left
Right
right
NotOutboard
non-outboard
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.