SeatBeltAnchorageBuilderLTwoLimitType Enumeration¶
NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilder.LTwoLimitType is an alias for NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderLTwoLimitType
-
class
NXOpen.Features.VehicleDesign.
SeatBeltAnchorageBuilderLTwoLimitType
¶ Bases:
object
the ltwo limit type
Enum Members
Enum Member Enum Member Description Degree45And80 L2 limit angle area between 45 degree and 80 degreeDegree50And70 L2 limit angle area between 50 degree and 70 degree-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-