SeatBeltAnchorageBuilderLOneLimitType Enumeration¶
NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilder.LOneLimitType is an alias for NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderLOneLimitType
-
class
NXOpen.Features.VehicleDesign.
SeatBeltAnchorageBuilderLOneLimitType
¶ Bases:
object
the lone limit type
Enum Members
Enum Member Enum Member Description Degree30And80 L1 limit angle area between 30 degree and 80 degreeDegree50And70 L1 limit angle area between 50 degree and 70 degree-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-