PedestrianProtectionBuilderWad Enumeration¶
NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder.Wad is an alias for NXOpen.Features.VehicleDesign.PedestrianProtectionBuilderWad
-
class
NXOpen.Features.VehicleDesign.
PedestrianProtectionBuilderWad
¶ Bases:
object
Settings for the start, end and boundary wrap around distance line to create
Enum Members
Enum Member Enum Member Description First First wrap around distance lineSecond Second wrap around distance lineThird Third wrap around distance lineFourth Fourth wrap around distance lineFifth Fifth wrap around distance lineSixth Sixth wrap around distance line. Not valid for boundary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-