MirrorCertificationBuilderMirrorSurfaceType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.MirrorSurfaceType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorSurfaceType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorSurfaceType

Bases: object

Used to indicate the mirror surface type.

Enum Members

Enum Member Enum Member Description
Planar
Represents the planar mirror surface
Spherical
Represents the spherical mirror surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.