MirrorCertificationBuilderMirrorOrientationType Enumeration

NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.MirrorOrientationType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorOrientationType

class NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorOrientationType

Bases: object

Used to indicate the method to rotate mirror.

Enum Members

Enum Member Enum Member Description
AutoRotation
Represents that the mirror will be rotated automatically
InteractiveAdjustment
Represents that the mirror will be rotated interactively
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.